The Mathematics of Log-Based Dynamic Processors
by THAT Corporation
Abstract
Dynamic Processors (compressors, expanders,
gates, etc.) may be easily constructed from THAT
Corporation Voltage-Controlled Amplifiers (VCAs)
and RMS-Level Detectors. The detector is used to
sense signal level and control the gain of the VCA to
produce compression or expansion. Both feedback
and feedforward configurations are possible.
Because these parts respond in logarithmic
fashion, developing a mathematical description of
circuits using them often leads to murky equations
which do little to clarify the circuit behavior. However, via an appropriate choice of units, the
mathematics can often be drastically simplified, resulting in surprisingly simple algebraic equations to
describe the circuit.
This application note describes the basis for
this mathematical treatment, and offers insights
into its application to circuit designs based on these
log-responding components.
The Mathematics of Log-Based Dynamic Processors
A dynamic audio processor is a device which ad
-
justs its gain to suit the requirements of the applied
audio signal. Dynamic processors include compres-
sors, expanders, noise gates, and similar devices.
All share the characteristic that their signal gain is
dependent on the input signal level in some fashion.
A compressor reduces its gain as the input signal increases, while a gate reduces its gain as the input signal
decreases. However, the basic concept of
varying gain to suit the requirements of the signal
remains unchanged.
At its most basic level, a dynamic processor
consists of a level sensor, a control-voltage processor and a voltage-controlled amplifier (VCA). The
level sensor produces a varying dc voltage representative of the signal level. The control-voltage processor
conditions this dc voltage, enabling it to control
the VCA gain as required. The VCA then adjusts the
signal gain based on the control voltage.
Many of the most popular dynamic audio processors have been constructed using THAT Corporation VCAs and THAT 2252
rms-level detectors. The
gain of a THAT215X or THAT218X VCA, and of the
VCA portion of a THAT4301 is exponentially dependent on its control signal. Conceptually this is
very simple: the VCA gain in decibels is directly
proportional to the control voltage applied. However, when expressed mathematically, it appears more
formidable:
where AV
is the gain of the VCA (in volts/volt), EC
is the applied control voltage, and VT
is the thermal voltage(kT/q) from the diode equation.
Figure 1: Block Diagram of a Feedforward Processor
Figure 2: Block Diagram of a Feedback Processor
The THAT 2252 rms-level detector and the rms-
level detector in the THAT 4301 share this simple-but-
complex characteristic. Their output signals are directly
proportional to the decibel level of their input signals.
Mathematically, this is further complicated by the time
response of the detector, but if one only considers the
steady-state condition, the math is as follows:
where VOUT
is the output voltage of the detector, and Virms
is the rms value of its input signal.
It is possible to write an equation which describes
the action of the simple dynamic processors shown in
Figures 1 and 2 using the logs and exponentials of
equations 1 and 2 above. However, this does not lend it-
self to illuminating the design process. The resulting
equation is difficult to solve in closed form, and, at
least to this author, does not offer insight into the ac-
tion of the processor.
Making the Math Simple
However, it is possible to greatly simplify the math
while adding to the meaning which it conveys. Consider
that, in audio products, it is the decibel level
of the signal which is most important, most relevant to our perception. By thinking about all the signal
voltages in the
circuit in terms of decibels, the mathematics can be reduced to simple algebra!
Consider the following equation:
This is equivalent to Equation 1, but expresses the gain, AdB
in decibels, not in linear terms (as was AV). It
clearly shows that the decibel gain of the VCA is directly
proportional to the control voltage EC . The constant
-166.7 is a scale factor deriving from the control voltage
sensitivity of approximately 6mV/dB.
Similarly, recognizing that the detector produces an
output proportional to the decibel level of its input signal, we can simplify Equation 2 in the same way:
In Equation 2a, VOUT
is the output of the detector, while dBRMS
is the decibel level of its input signal.
Armed with the revised Equations 1a and 2a, let us
mathematically explore the action of the processors in
Figures 1 and 2.
Feedforward Processor Math
For Figure 1, the feedforward processor, the output
signal level is equal to the sum of the input signal level
and the VCA gain. (While the VCA multiplies the input
signal by its linear gain, in the logarithmic world this reduces to
addition.) Mathematically, this is:
where dBOUT
is the VCA's output level, dBIN
is its input level, and AdB
is its gain (all in decibels, of course).
The VCA gain is determined by the control voltage
applied to it, which depends on the detector's output
voltage and the control-voltage processor gain. From
equation 2a and the block diagram, the applied control
voltage, EC , is:
Combining Equations 1a, 3 and 4, we can solve for the output level:
This simple equation points out the inherently linear re-
lationship between decibel input and output levels in dy-
namic processors based on THAT Corporation VCAs
and rms-level detectors.
Compression/Expansion Ratio
In compressor and expander design, the ratio of input level changes to output level changes is frequently
referred to. This is called the compression ratio (or expansion ratio ). We can rearrange Equation
5 above to
solve for the ratio of the feedforward dynamic processor, as follows:
Equation 6 shows that the compression or expansion ratio depends only on the gain in the controlvoltage processor
placed between the detector output
and the VCA input. Moreover, whether the processor is a compressor or an expander depends on G.
For G=0, the ratio is unity - as would be expected,
no dynamic processing takes place. For 1>G>0, the
output is less than the input, so the processor is a compressor. For G<0, the output is greater than the input,
so the processor is an expander. For G>1, the ratio becomes negative, which results in "negative
compression." In this configuration, the output
decreases as the input increases. The dynamic inversion thus produced
sounds somewhat like playing a tape backwards.
Feedback Processor Math
For Figure 1, the feedback processor, the math is
slightly different. Equation 3 still holds, because the
signal path is not changed from that in the feedforward
processor. However, the control voltage, EC , is based on
the output level, not the input level. Therefore, from
Equation 2a and the block diagram:
Combining Equations 1a, 3 and 7:
Rearranging terms:
This relationship is nearly as simple as Equation 5
for the feedforward processor.
The ratio can be easily extracted from Equation 9:
Note the differences between Equation 10 (feed-
back) and Equation 6 (feedforward). The feedback
processor is a compressor for G>0, and an expander
for G<0. The ratio function contains a singularity at
G=-1: at which point the expansion ratio is infinite
(and the circuit is unstable!). Infinite compression re-
quires infinite G (and is therefore impossible to
achieve, though it is possible to get close).
Practical Dynamic Processors - Introducing a Threshold
As shown, the processors in Figures 1 and 2 form
simple, linear companders. Assuming G is constant, all
signal levels, large and small, are subjected to the same
ratio. For application as an audio effects device, a practical compressor requires a threshold below which
processing stops in order not to bring up noise during
pauses in the signal. A noise gate (or expander gate) requires a threshold above which the processing stops in
order to pass desired signals without change.
These objectives are easily met by providing a non-linear circuit which changes the value of G based on the
output of the detector. A simple silicon diode rectifier in
the control-voltage path will produce a broad transition
between regions of processing and no processing. The
width of the transition region may be controlled by amplifying the control voltage before passing it through the
diode, and attenuating it afterwards. An operational
half-wave rectifier (which linearizes and sharpens the
diode characteristic by placing it in the feedback loop of
an opamp) will produce a sharp transition between regions of processing and no processing.
It is possible to combine several types of control-
voltage processing into one circuit, by using diodes to
switch control-voltage processor paths based on the
output voltage from the detector. For example, in a feed forward processor, G could be set less than 0 for low
values of dBIN , and set greater than 0 for high values of
dBIN . This would produce expansion (or gating) below
one threshold, and compression above another. More
than one compression ratio may be selected, depending
on signal level, by providing more than one threshold
with multiple, positive values of G. The combinations
are limited only by the imagination of the designer.
Mathematically, the effect of adding a nonlinear circuit as discussed above is to split the ratio equation
into two or more individual equations, each of which
holds only in a specific region of operation. For a typical, sharp-threshold, feedforward, above-threshold
compressor, the mathematics would look like this:
For a more detailed look at these circuits applied to
compressors, see AN100A, Basic Compressor/Limiter Design, also available from THAT Corporation.
Feedback vs. Feedforward
In choosing between a feedback and feedforward
processor design, there are several factors which will
influence the decision. There is no simple way to determine which is the best approach, and the designer
must weigh the factors in light of the design objectives.
Detector Dynamic Range
In feedforward processors, the level detector is exposed to the entire dynamic range of the input signal.
The THAT 2252 provides accurate audio-band rms-to-dc conversion over a 60dB dynamic range, extending to
80dB over a more limited bandwidth. The THAT 4301
Detector has even wider dynamic range. For an above-threshold compressor, this will present little problem
since processing is restricted to the dynamic range
above threshold (usually less than 60dB).
A feedback compressor has the advantage that the
dynamic range at the detector is reduced by the compression action. The feedback configuration was chosen
for dbx Type I and II noise reduction encoders (compressors) partly because of this factor. There, the
compression ratio is 2:1, with no threshold of compression
(except for frequency shaping, the block diagram resembles Figure 2 quite closely). By placing the detector
at the output of the compressor, the dynamic range it
must handle is reduced by one-half, allowing a 60dB
detector to accommodate 120dB of input dynamic range.
Available Ratios
However, the feedback configuration has the disadvantage that not all compression ratios are possible.
The high level of feedback required to reach high compression ratios makes feedback processors more likely
to exhibit instabilities if high compression ratios are allowed. Instability is also likely in feedback
expanders
where high expansion ratios are desired (e.g., noise gates). An additional drawback is that negative compression
ratios are not possible. By contrast, all this is
possible in feedforward.
Time Constants
While this discussion has not addressed the effect
of the detector's time constant on a dynamic processor,
it is worth noting that the configuration chosen will affect the processor's transient response. Consider that
in
either type of compressor, the output will overshoot on
sudden transients unless the detector response is instantaneous. The detector in the feedback compressor
sees this overshoot, which will modify its response behavior. The detector in the feedforward compressor
sees only the input signal, and acts accordingly.
Mirror-Image Symmetry
Certain types of dynamic processors are intended to
be used in paired applications, such as the combination
of a noise-reduction encoder which is paired wi th a decoder. In this case, the processing of the encoder, (a
compressor) is intended to be inverted, or "un-done" by
the decoder (an expander). It is possible to exploit the
mirror-image symmetry between feedback and feedforward configurations to help ensure accurate decoding
during the expansion process.
Consider the case of the block diagram of Figure 2
(feedback) configured as a compressor, and the block
diagram of Figure 1 (feedforward) configured as an expander. If the feedback compressor is used as the encoder,
and the feedforward expander as the decoder, a
"back-to-back" connection of the two devices would
have the output of the feedback circuit connected directly to the input of the feedforward circuit. In this
arrangement, the detectors in each circuit are connected
to the same signal, so their responses will be identical
over time and level variations, provided the detectors
themselves match.
If both processors were feedforward, the detectors
would see different signals (the compressor sees its input, the expander sees the compressor's output). With
two feedback processors, the detectors again see different signals. Therefore, to provide optimum tracking in
encode-decode processor applications, a combination
of feedback encoder with feedforward decoder is recommended to provide the best chance for accurate
mirror-image processing. (This is one reason why dbx Types I and II and dbx-TV noise reduction use this
mirror-image principle in their designs.)
Summary
While at first appearing somewhat formidable, the
mathematics of log-based dynamic processors reduces
to relatively simple, algebraic equations. Happily for the
designer, the constants in the mathematics have clear
and direct relation to the circuit elements and performance. Compression and expansion ratios, in particular,
are amenable to straightforward mathematical solutions and circuit implementations.
Nonlinear circuits (diodes, operational rectifiers
and the like), may be used to provide thresholds
(breakpoints in the transfer characteristic). Single and
multiple thresholds may be accommodated via the
same mathematical analysis.
Feedforward and feedback processors have individual strengths and weaknesses, and in choosing between
them the designer should consider such diverse elements as dynamic range, required ratios of compression or
expansion, target time constants, and the need
for mirror-image symmetry between compressors and expanders.